AXIS#.WS.DISTMAX

Description

This parameter sets the maximum movement that is allowed for finding commutation. If this value is too small,F5501, "Wake and Shake - Excess movement.", may occur before wake and shake is finished. The larger this value, the more movement is allowed for wake and shake. This value is application dependent.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

deg (position units)

Range

0 to 90 deg

Default Value

15 deg

(missing or bad snippet)

Float

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.WS.DISTMAX

5013h

0ch

Signed32

Position

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6701

1

6701 (0x1a2d)

AXIS1.WS.DISTMAX

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.WS.DISTMAX

6701

Signed32

Read/Write

Position